Technical FAQs

Ask a Question

What are the changes in client licenses for Vijeo Citect V7.30.

With the release of new Vijeo Citect V7.30 the distinction between Web and non-Web client versions has been removed.
The difference between the Control and View-only client types remains. The Control Client license enables both standard
and web variants of the clients in the software to run. Likewise for the View-only Client license.

The Web version part numbers have been removed from the standard offer and are only available for legacy versions of the product.
Was this helpful?
What can we do to improve the information ?