Technical FAQs

Ask a Question

What is the idle logout time of Vijeo Citect logged-in user.

The user will not automatically logged out bydefault , either you need to call Logout() function or need to configure LogoutIdle() function
which will automatically logged out the user as per the time that you have set in the function like for LogoutIdle(5), the user will be logged
out after 5 minutes if the current user does not execute any command .
Was this helpful?
What can we do to improve the information ?