Technical FAQs

Ask a Question

What is difference between floating point and static point licensing in Vijeo Citect.

A client license can be static or floating depending on requirements

Static client license: For operators needing access to the system at all times, irrespective of the number of
connections already established by other clients.
A static client license provides permanent access to the system, as
it physically resides in the key plugged into the client PC.

Floating client license: Users who occasionally need to use a client
for operator tasks can purchase floating licenses. Connections will be allowed until the number of valid licenses is reached.
Floating client licenses are stored on the key plugged into the server machine.
Was this helpful?
What can we do to improve the information ?