Technical FAQs

Ask a Question

Is it possible to enable "Auto Scrolling" for the EM6400 series meter display.

Auto Scroll allows the user to monitor a group of Display Pages sequentially, every 5 seconds, without constant key pressing.
 
There are three different auto scrolling modes:
 
1. To auto scroll within a specific page group (RMS, THD, INTG, etc..):
Navigate to a particular page in the desired page group, then press the up key continuously for 3 seconds and release.
The display will flash AUTO and start to auto scroll within the page group.
 
2. To auto scroll down the entire column of pages:
Navigate to the desires page, then press the down key continuously for 3 seconds and release. The display will flash AUTO
and start to auto scroll through the entire column of pages.
 
3. To auto scroll through TURBO pages:
Press the TURBO key continuously for 3 seconds and then release.The display will flash AUTO and start to auto scroll through
the TURBO pages.
 
The TURBO pages consist of the following values:
VLL, A, PF
VLN, A, F
VA, W, PF
VA, W,VA
W, VAR, PF
PF1, PF2, PF3
V% 1 2 3
A % 1 2 3
VAd RD TR
MD HR
VAh, Wh
RVAh, RWh
tVAh, tWh
 
Press any key to revert back to manual scrolling.
Was this helpful?
What can we do to improve the information ?