Technical FAQs

Ask a Question

How many stop bits does the EGX support.

All EGX devices use an 11-bit frame serial frame. 1 start-bit, 8 data-bits, and 1 or 2 stop bits
depending on the parity selection.
 
Even parity: 1 Stop-Bit, 8 Data-Bits, 1 Parity-Bit, 1 Stop-Bit
Odd parity: 1 Stop-Bit, 8 Data-Bits, 1 Parity-Bit, 1 Stop-Bit
No parity: 1 Stop-Bit, 8 Data-Bits, 2 Stop-Bits.
Was this helpful?
What can we do to improve the information ?