Technical FAQs

Ask a Question

What's the burden of BCPM power consumption.

 The BCPM is fused at 500mA so, that will be the absolute maximum it could draw, however we expect normal draw to be less than 100mA.
So if the voltage supply is 220 V, then the burden will be 220 x 0.1=22 VA
Was this helpful?
What can we do to improve the information ?