Technical FAQs

Ask a Question

What is maximum length of the cable between MCB and Acti9 Smartlink.

The cable length between an input of the Acti9 Smartlink and any device connected is limited to 20 meters.
Was this helpful?
What can we do to improve the information ?