Technical FAQs

Ask a Question

Is it necessary to connect the Acti9 range of contactor (iACT24) to the 230VAC power supply.

The 24VDC is just used to send the command, from Acti 9 Smartlink or a PLC. To be able to energize the coil of the
associated contactor, the iACT24 must have its P (phase) and N (neutral) terminals connected to the 230VAC power.
Was this helpful?
What can we do to improve the information ?