Technical FAQs

Ask a Question

What is the Flashing C on the ATV21 and ATV212 drives?

Issue:
Display is flashing "C"

Product Line:
ATV212, ATV21

Environment:
All Models and serial numbers

Cause:
Motor is drawing excessive current or the motor settings in the drive are incorrect.

Resolution:
Flashing C means the drive is in a current limit state. 
Check F601 current limit setting.  It should be set to 1.2 X motor FLA.
If motor amps still reaches the F601 value, suspect a motor or load problem.
Was this helpful?
What can we do to improve the information ?