Technical FAQs

Ask a Question

What is the difference between pre-cabled connectors (1) XZ CP1141L2 and (2) XZ CP1169L2 when both are 4 pins, female, straight and M12 connectors.

 Difference between (1) XZ CP1141L2 and (2) XZ CP1169L2 is as below.
 
==> XZCP1141L2 is a straight, 4 pins M12 Female connector with PUR cable of 2 meter length with cable outer diameter 
      of 5.2 sq. mm and total weight of 0.09 Kg
 
==> XZCP1169L2 is a straight, 4 pins M12 Female connector with PUR cable of 2 meter length but with cable outer diameter
      of 5.7 sq. mm and total weight of 0.105 Kg. Also, this pre-wired connector having 4 pins that includes earth pin also.
Was this helpful?
What can we do to improve the information ?