Technical FAQs

Ask a Question

Can any of the patch or update regarding library applied to SoMachine be removed individually from SoMachine.

Any of the patch or update regarding library applied to SoMachine can not be removed individually from SoMachine. Either
of them can be removed only with complete un-installation of SoMachine and Solution extension (if installed).
Was this helpful?
What can we do to improve the information ?