Technical FAQs

Ask a Question

Is it possible to download program to M218 controller via Ethernet port.

Connectivity between M218 controller – Ethernet port and PC running SoMachine (version v3.1 SP1 or any earlier version) is not possible
because this feature is not available in SoMachine for M218 controller. So, option is to do program via USB port of M218 controller.
Was this helpful?
What can we do to improve the information ?