Technical FAQs

Ask a Question

What kind of Technology is used in Type 1 and Type 2 class of surge arresters.

The Type 1 (PRF1 surge arresters) use “encapsulated air-filled spark gap “ type technology without arc device while as the
Type 2 (PRD surge arresters) use “varistor” type technology or “varistor + gas-filled spark gap” technology.
Was this helpful?
What can we do to improve the information ?