Technical FAQs

Ask a Question

What is the part number for the USB cable to connect a PC to a drive or soft start when using SoMove or Powersuite?

Issue:
What is the part number for the USB cable to connect a PC to a drive or soft start when using SoMove or Powersuite?

Product Line:
ATV Altivar ATS Altistart

Environment:
All current products

Cause:
Needs a USB cable to connect a PC to an Altivar/Altistart when using Somove software.

Resolution:
TCSMCNAM3M002P:  This cable is a USB to RS485 interface cable to be used with SoMove and Powersuite.
Was this helpful?
What can we do to improve the information ?