Technical FAQs

Ask a Question

After installing Service Pack-1 for ION E 6.0, OPC client will not connect to the server.

The "OPC Data Access Server Service" not exist in services.  Need to register it manually.  At a cmd prompt, type 'ION.OpcDaServer.exe -Service'
and should reappear. You will have to start it up and change the Start up type from Manual to Automatic.
Was this helpful?
What can we do to improve the information ?