Technical FAQs

Ask a Question

Is it possible to read single phase meters as well as three phase meters modbus registers at the same time from BCPM

Yes, there should be no problem to read the SINGLE-PHASE METERS MODBUS POINTMAP as well as 3-PHASE METERS MODBUS POINT MAP at the same time.
Was this helpful?
What can we do to improve the information ?