Technical FAQs

Ask a Question

What is the current rating for a ZBE101 contact?

Depends on voltage, see attached.
AC1 240v = 10A
AC15 240v = 3A
DC13 125v = 0.55A
Was this helpful?
What can we do to improve the information ?