Technical FAQs

Ask a Question

Is it possible to use NSX200NA DC PV in a circuit where minus pole is solidly earthed and to open and close plus pole only by 4 poles connected in series.

The NSX200NA DC PV switch disconnector can be used in a circuit where minus pole is solidly earthed.Then it can open and close only plus pole by 4 poles connected in series.
Was this helpful?
What can we do to improve the information ?