Technical FAQs

Ask a Question

Is it possible to use limit switch ZCKJ1H29 to switch a 400V ac coil on a starter?

 Yes, at 0.5Amp and 400V you can expect about 600,000 operational cycles out of the limit switch which has a 500V insulation voltage rating.
Was this helpful?
What can we do to improve the information ?