Technical FAQs

Ask a Question

What is the part code for a 5 meter cable for a XS1M12PAW01D Inductive Proximity Sensor?

This prox requires a 4 pin M12 female connector, the item required will depend on the environment.
The part code for a 4 pin M12 pre wired female straight connector with PVC flex is XZCPV1141L5 (angled option = XZCPV1241L5)
The part code for a 4 pin M12 pre wired female straight connector with PUR flex for severe environments is XZCP1141L5
The part code for a 4 pin M12 pre wired female straight connector for food & beverage applications is XZCPA1141L5 (ANGLED OPTION = XZCPA1164L5)
2 or 10m options may also be available
See attached data sheet
Was this helpful?
What can we do to improve the information ?