Technical FAQs

Ask a Question

What is the connector to fit the XUM2AKCNM8T proximity switch

The connector is an M8 4 pin female connector
XZCPV0941L2 for a straight connector with PVC cable
XZCPV1041L2 for an angled connector with PVC cable
XZCP0941L2 for a straight connector with PUR cable for severe environments
XZCPA0941L2 for a straight connector for food & beverage applications
(change L2 to L5 or L10 for 5 or 10m cables)
See attached data sheet
Was this helpful?
What can we do to improve the information ?