Technical FAQs

Ask a Question

Can we edit the Data backup file (*.DTX, *.DAT) saved by Unity Pro using notepad or any other software.

There is no possibility to modify the data file whether it is *.DAT or *.DTX using any other tool because it is specific binary file which can only
 be edited by Unity Pro.  The option for you to edit this file is as follows: 

1. Open Unity Pro application and run it in simulation mode. 
2. Restore the *.DTX or *.DAT file and then modify the values using animation table. 
3. Save the data file again in the PC. 
4. Connect the Unity to PLC using Standard mode and then again transfer new data file into PLC. 
Was this helpful?
What can we do to improve the information ?