Technical FAQs

Ask a Question

We are getting errors Error in AddStatusElement while starting Web View on PLS v7.20 system with IE 10.

Internet Explorer 10 does not allow XML storage which is used in the SCADA webclient. The SCADA webclient will only be
supported with Internet Explorer 10 in SCADA 7.3 Spk1 onwards.  In SCADA webclient v7.30 and below, Internet Explorer 10
is not supported and you will get the error "Error in AddStatusElement():" You need to degrade your IE 10 to IE9 or any older
versions to view web client easily.  
Was this helpful?
What can we do to improve the information ?