Technical FAQs

Ask a Question

What is the part code for a Phase failure RELAY to operate on 400V

If it is to be used in a motor protection then the RM4TA02 or 32 should be used
The 02 has a fixed 0.5s delay, the 32 has an adjustable 0.1 - 10s delay
See attached data sheets.
Was this helpful?
What can we do to improve the information ?