Technical FAQs

Ask a Question

Does the Harmony 3 position Rotary Switch activate the centre contact if fitted?

No, the selector switches can't activate a center contact.
If required you could install the opposite contact on both sides and wire them in series or parallel to activate as required when the switch is in the centre position.
Was this helpful?
What can we do to improve the information ?