Technical FAQs

Ask a Question

Which type of SF6 circuit breakers is equipped with pressure switches.

SF1 type 1 pole units (630 A) cannot be equipped with a pressure switch.
SF1 type 2 (1250 A) and SF2 circuit breaker pole units can be equipped as an option.
All Circuit breakers in the LF range are equipped with a pressure switch as standard.
Was this helpful?
What can we do to improve the information ?