Technical FAQs

Ask a Question

What is the maximum angle at which CT Contactor can be mounted for normal operation.

The maximum allowable angle at which CT Contactor can be mounted in relation to the normal vertical mounting plane from the rail is 45°.
Was this helpful?
What can we do to improve the information ?