Technical FAQs

Ask a Question

Is it possible to mount C60 range of MCBs Works in Horizontal Position.

Yes, The C60 range Modular Circuit Breaker (MCB) will work without any effect on its performance if mounted in Horizontal Position.
Was this helpful?
What can we do to improve the information ?