Technical FAQs

Ask a Question

Is it possible to use the ID range of RCCB when mounted in Horizontal Position.

Yes, The Multi9 Residual current Circuit Breaker (RCCB-ID) will work without any effect on its performance if mounted in Horizontal Position.
Was this helpful?
What can we do to improve the information ?