Technical FAQs

Ask a Question

How can I run Vijeo Citect on system startup.

To run Vijeo Citect on startup first select the project in Citect Explorer and then run computer setup wizard and finish it. Then open the
Windows Startup folder and add the Vijeo Citect Runtime from the start menu in the Startup folder as shown.

Was this helpful?
What can we do to improve the information ?