Technical FAQs

Ask a Question

How to setup a control client in Vijeo Citect.

To make a control client you need to restore the project backup of the Server system on client machine. You need to also make sure
that in your project you have configured the network address of the Vijeo Citect Server system. Then after restoring the project run the
computer setup wizard and then start the runtime as control client.
Was this helpful?
What can we do to improve the information ?