Technical FAQs

Ask a Question

What are the dimension A and B when the interphase barriers are fittted on the Compact NS630b-1600 circuit breaker.

 The dimensions are A=185 mm and B= 80 mm when the interphase barriers are fitted on the Compact NS630b-1600 circuit breaker.
Was this helpful?
What can we do to improve the information ?