Technical FAQs

Ask a Question

Can the head on 9007C limit switches be rotated?

ISSUE
Can the head on 9007C limit switches be rotated 180 degrees?

PRODUCT LINE
Limit switches

ENVIRONMENT
9007C

CAUSE
Adjustments or modifications 

RESOLUTION
Yes, the head can be rotated 360 degrees in 90 degree increments.
Was this helpful?
What can we do to improve the information ?