Technical FAQs

Ask a Question

What is the difference between ZBRRC and ZBRRA?

Issue:
What is the difference between ZBRRC and ZBRRA?

Product Line:
Push Buttons

Environment:
NEMA 1,4, 4X 12

Cause:
Product Selection

Resolution:
ZBRRC has 4 programmable PNP outputs rated at 200mA. The ZBRRA has 2 programmable relay outputs and is rated at 3A.
Was this helpful?
What can we do to improve the information ?