Technical FAQs

Ask a Question

Kindly confirm if clear incandescent bulb DL1CE130 can be used on 120VDC. The product catalog did not mention the type of voltage, but in the datasheet it was only for AC.

Yes, you can use this clear incandescent bulb DL1CE130 with 120-130 VDC 2.4W also, actually an incandescent bulb has not polarity, that means you can use them either in AC or in DC voltage.  
Was this helpful?
What can we do to improve the information ?