Technical FAQs

Ask a Question

What is the maximum numbers of wireless and Battery less radio transmitters that can be connected with ZBRN1 (Modbus TCP/IP protocol) / ZBRN2 (Modbus serial protocol) access points.

ZBRN1 (Modbus TCP/IP protocol) / ZBRN2 (Modbus serial protocol) access points can support maximum up to 60 numbers of Radio transmitters.
Was this helpful?
What can we do to improve the information ?