Technical FAQs

Ask a Question

Is it possible to reset the Energy Value (Wh, VAh & VARh) from SCADA through Modbus communication in EM6400 multifunction energy meter.

Integrator (INTG) and demand clearing and setting up the setup default i.e. "CLEAR BLOCK" parameters through modbus communication are not available in EM6400 series multifunction meter, this is to be done via. meter front panel.
Was this helpful?
What can we do to improve the information ?