Technical FAQs

Ask a Question

How to reset the Energy Value (Wh, VAh & VARh) from SCADA through Modbus communication in PM100 series power meter.

Integrator (INTG) and demand clearing and setting up the setup default i.e. "CLEAR BLOCK" parameters through modbus communication available in PM1000 series power meter.
Refer the attached "
Clear Block.PNG" for Parameter, Modbus Register Address, Data Type & Range for Integrator (INTG) and Maximum Demand Clear.
Was this helpful?
What can we do to improve the information ?