Technical FAQs

Ask a Question

ATS48 soft starter internal fan part numbers.

Issue:
Does the Altistart 48 soft start have an internal fan?

Product Line:
Altistart 48

Environment:
All models, all serial numbers

Cause
Replacement and repair pars

Resolution:  
The following list shows the softstart part number along with the part number and (quantity) of the fan kits needed for each softstarter. 


ATS48D32Y - VZ3V481 (1)
ATS48D38Y - VZ3V481 (1)

ATS48D47Y - VZ3V4811 (1)

ATS48D62Y - VZ3V482 (1)
ATS48D75Y - VZ3V482 (1)
ATS48D88Y - VZ3V482 (1)
ATS48C11Y - VZ3V482 (1)

ATS48C14Y - VZ3V483 (1)
ATS48C17Y - VZ3V483 (1)

ATS48C21Y - VZ3V484 (1)
ATS48C25Y - VZ3V484 (1)
ATS48C32Y - VZ3V484 (1)

ATS48C41Y - VZ3V485 (1)
ATS48C48Y - VZ3V485 (1)
ATS48C59Y - VZ3V485 (1)
ATS48C66Y - VZ3V485 (1)

ATS48C79Y - VZ3V485 (2)
ATS48M10Y - VZ3V485 (2)
ATS48M12Y - VZ3V485 (2)



 
Was this helpful?
What can we do to improve the information ?