Technical FAQs

Ask a Question

ATV212: Can the default display value be changed from output frequency to another value?

ATV212:  The default display shows output frequncy.  Can it show motor current?

Product line:
Altivar 212

All models, all serial numbers

Customer preference

Parameter F710 sets the default display.  The factory setting is 0 for motor operating frequency. Other options:
1 = speed reference
2 = motor current
3 = drive rated current
4 = drive thermal state
5 = output power
6 = PID internal speed reference
7 = serial comm data
8 = output speed
9 and 10 are communication frames received data
Was this helpful?
What can we do to improve the information ?