Technical FAQs

Ask a Question

Does Sepam Series 80 model B83 relay has fuse failure protection feature.

Protection against fuse failure i.e. "VT Supervision" ANSI code - 60FL is available in B83 & B80 Sepam 80 series range.
Was this helpful?
What can we do to improve the information ?