Technical FAQs

Ask a Question

What is the maximum inrush current allowed by the ATS48?

Issue:
Specifications for maximum inrush current

Product Line:
Altistart , ATS48

Environment:
All models , all serial numbers

Cause:
Want to increase the current limit on startup.

Resolution:
ATS48 Current limitation setting, will allow up to 700% of the IN (FLA) setting.
Was this helpful?
What can we do to improve the information ?