Technical FAQs

Ask a Question

ATV32 - Does it have Brake Logic control?

Issue:
ATV32 - Does it have Brake Logic Control?
Product line:
Altivar ATV32
Environment:
All models, all serial numbers
Cause:
Basic features for the ATV32 drive.
Resolution:
ATV32 does have Brake Logic Control. 

Refer to the ATV32 Programming manual, ATV32_programming_manual_S1A28692_01
Was this helpful?
What can we do to improve the information ?