Technical FAQs

Ask a Question

How can one reset the KW consumption on an ATV212 with Metasys N2 communications?

Issue:
How can one reset the KW consumption on an ATV212 with Metasys N2 communications?

Product line:
Altivar ATV212

Environment:
All models, all serial numbers

Cause:
Need to reset energy counter

Resolution:
With Metasys, you are using a BACnet protocol. By writing a value in AV#8, the energy counter should be reset.

Refer to the ATV212 Metasys N2 manual ATV212_Metasys manual_N2_EN_S1A53846_01

Was this helpful?
What can we do to improve the information ?