Technical FAQs

Ask a Question

How to join two strings with result more than 16 characters in Unity Pro.

By default the maximum characters allowed for the STRING data type is only 16. It can be increased to 65534 ASCII characters.
 For this select the data type as STRING [<size>], where size denotes an unsigned integer (UINT) capable of defining a string
between 1 and 65534 ASCII characters.
Was this helpful?
What can we do to improve the information ?