Technical FAQs

Ask a Question

What is the accuracy of the Premium PLC CPU real time clock

Real time clock accuracy:

Accuracy of the real time clock is one second (%SW50) +/- 200ms.

Resolution of the real time clock is one second (%SW50) +/- 200ms,because 200ms is the refresh rate of the RTC.
 
Accuracy error:
 
The accuracy error of the quartz oscillator is:
 
1. At 0 and 70°C : -101/20 ppm, error in second/day is -8.7/1.7, in minute/year is -53/11.
 
2. At 25°C: -20/20 ppm, error in second/day is -1.7/1.7, in minute/year is -11/11.
 

Was this helpful?
What can we do to improve the information ?