Technical FAQs

Ask a Question

Where is the location of the Elementary Function Block (EFB) library in concept V2.6.

EFB library gets loaded automatically when Concept is installed and is available at the location x:\Concept\Lib.(Where, 'x' is the root directory).

Was this helpful?
What can we do to improve the information ?