Technical FAQs

Ask a Question

How can I save the public variables of a DFB with PL7-PRO

The public variables of a DFB can be modified by program or with animation tables. When reloading programs, these public variables return to the
initialisation values defined in the DFB editor. To retain the modified values, the S box of the variables concerned must be checked (in the DFB editor)
and system bit %S94 set to 1. The public variables are then saved.
Was this helpful?
What can we do to improve the information ?