Technical FAQs

Ask a Question

What is difference between X80 BMX CRA 312 00 and BMX CRA 312 10.

CRA31200 is a standard module for small drops with basic functions and no expert modules can be configured with this drops.
CRA31210 is the performance module with support to higher number of IO's and capability of handling expert modules ( NOM, ERT, EHC ).
CRA31210 also includes Time stamping at 10 mS, supports Change Configuration on the Fly ( CCOTF ).
Was this helpful?
What can we do to improve the information ?