Technical FAQs

Ask a Question

How many ERT modules can be used on a X80 drop.

The maximum number of expert channel supported on a X80 drop is 36.
One BMXERT has 16 inputs and counts as 4 expert channels. So total no. of ERT modules that you can plug in a X80 drop is 36/4 = 9 Nos.
Was this helpful?
What can we do to improve the information ?